Technical FAQs

Ask a Question

What is the Current Consumption and lifespan data for RZM031BN LED

Issue:
What is the Current Consumption and lifespan data for RZM031BN LED

Product Line:
Zelio Relays, Plug in Relays, Industry, RSB interfact Relays

Environment:
Global

Cause:
Possibility of leakage current as well as device consumption requirement

Resolution:
The current consumption of RZM031BN module are approximately:
24Vdc = 2mA 
48Vdc = 4mA
60Vdc = 5mA

And the LED lifespan is up to 100 000 hours, at rated voltage and at an ambient temperature of 25 °C.
Was this helpful?
What can we do to improve the information ?