Technical FAQs

Ask a Question

What's the replacement of the LMC20 motion controller?

Issue:
What's the replacement of the LMC20 motion controller?

Product Line:
LMC20

Resolution:
The LMC20 is replaced by the LMC058 motion controller.
This is not a direct replacement so if additional IO or communication cards are needed, those will have to be added to the LMC058.
Also, the LMC20 uses the Motion Pro software while the LMC058 uses the SoMachine software so the program will have to be manually converted to SoMachine.
Was this helpful?
What can we do to improve the information ?