Technical FAQs

Ask a Question

S135 Form Code

Issue:
What is the S135 suffix for an an LC1D contactor?

Product Line:
IEC Contactors - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
This S135 suffix is an older form that was not offered in the US, though it may show up on imported equipment.  When it was offered overseas, it was a contactor where the standard coil suppressor was removed and a blanking piece was inserted instead.  
Was this helpful?
What can we do to improve the information ?