Technical FAQs

Ask a Question

Is the DU321RB CSA or only UL listed?

Product Line:
Safety Swiches

Environment:
DU,CHU

Resolution:
No, the DU switches are only UL listed, we have no equal in the Canadian version, for unfused switches they would have to use a Heavy Duty unfused switch CHU36*RB.
Was this helpful?
What can we do to improve the information ?