Technical FAQs

Ask a Question

Varistor Suppressors for RUM Relays

Issue:
Is there a 120V Varistor for the RUM relays?

Product Line:
General Purpose Relays - GIC Product

Environment:
US Product

Cause:
Product Accessories

Resolution:
No, only 240Vdc and 24Vdc Varistor suppressors are available.  An RC circuit suppressor for 110-240Vac and a Diode suppressor for 6-250Vdc are available though.
Was this helpful?
What can we do to improve the information ?