Technical FAQs

Ask a Question

TeSys T - Firmware Version of New Units

Issue:
Are all units that are shipped new of the same firmware version?

Product Line:
TeSys T Motor Management - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
Yes, all units in warehouse are upgraded when new versions of firmware are released and all new units are manufactured with the latest version available.
Was this helpful?
What can we do to improve the information ?