Technical FAQs

Ask a Question

XPSVNE3442P - Can this be used for 600VAC

Issue:
Can the XPSVNE be used on applications with a line voltage of 600VAC (575VAC)?

Product Line:
Safety relays, Preventa, 

Environment:
North America Products

Cause:
Catalog data shows a maximum of 500V (rms)

Resolution:
The XPSVNE cannot be used in this kind of application!

To limit the input voltage below the allowed range, customer would have to use a pre-resistor of minimum 270kOhm.
Unfortunately with such a resistor the XPSVNE will detect a wire broken and so will not be able to switch the outputs in case of real standstill.

 
Was this helpful?
What can we do to improve the information ?