Technical FAQs

Ask a Question

Dual Action Transmitter for Harmony Wireless

Issue:
How does the dual action wirless transmitter differ from the standard wireless transmitter?

Product Line:
Harmony Wireless, Batteryless Push Buttons - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The standard action transmitter sends a single pulse when the button is depressed, and no signal when the button is let go.  The dual action transmitter sends one momentary pulse when the button is depressed, and sends a second momentary signal when the button is let go.  This action mimics a momentary hardwired button which is held down by an operator.  
 
Was this helpful?
What can we do to improve the information ?