Technical FAQs

Ask a Question

Why are all of the lights off on my Conext SW?

Issue:
Conext SW won't stay on; all of the lights turn off shortly after starting

Product Line:
Conext SW hybrid inverter/chargers

Environment:
Any new Conext SW installation

Cause:
Initial startup behavior not described in manual

Resolution:
When the Conext SW is first started, the inverter is disabled
As a result, in a standard off-grid installation, all of the lights will turn off right after bootup
Use the SCP or ComBox to enable the inverter and/or the units front panel display
Was this helpful?
What can we do to improve the information ?