Technical FAQs

Ask a Question

What is the maximum branch breaker that a 14" wide NQ panelboard will accept?

Issue:
What is the maximum branch breaker that a 14" wide NQ panelboard will accept?

Product Line:
NQ panelboards sold and supported in the USA.

Environment:
Application

Cause:
Selection

Resolution:
The maximum breaker that can be installed in a 14" wide NQ panelboard is 100A. 
 
 
Was this helpful?
What can we do to improve the information ?