Technical FAQs

Ask a Question

How many Conext SW can be stacked in my solar system?

Issue:
Customer wants to have more than on Conext SW in their solar system.
 
Environment:
Solar System
 
Cause:
Need to have more than one inverter/charger in solar system.
 
Resolution:
Multiple unit configuration allows two inverter/chargers to operate in parallel doubling the capacity in inverter mode.
 
Additional Information:
More information on multiple unit charging can be found on page 1-5 of the manual. To download the manual use the following link http://solar.schneider-electric.com/wp-content/uploads/2015/09/Conext-SW-NA-Owners-Guide-120-240VAC-975-0638-01-01_Rev-E_ENG.pdf
Was this helpful?
What can we do to improve the information ?