Technical FAQs

Ask a Question

What voltage do I need to start the MPPT80 600?

Issue
How many solar panels do I need to use the MPPT 80 600?

Environment
Any installation with the MPPT 80 600

Product Line
MPPT 80 600

Cause
The MPPT 80 600 is a high voltage charge controller and has a very specific range of where it will work.

Resolution.
Solar panel voltage will vary depending on the brand on the model.  The Maximum Power Voltage (Vmp) of the combined panels in series needs to be above 230V to start the controller.  Once started, the MPPT 80 will operate between 195V and 550V.
Was this helpful?
What can we do to improve the information ?