Technical FAQs

Ask a Question

Can File Transfer be done in ATS22 using Remote Keypad?

Issue:
Can File Transfer be done in ATS22 using Remote Keypad?

Product Line:
ATS22, Altistart 22

Environment:
All

Cause:
NA

Resolution:
No. File transfer cannot be done with Remote Keypad. Need SoMove Software or Multiloader for that purpose.
Was this helpful?
What can we do to improve the information ?