Technical FAQs

Ask a Question

Can parameters be locked or password protected on ATS22 Softstart?

Issue:
Can parameters be locked or password protected on ATS22 Softstart?

Product Line:
ATS22, Altistart 22

Environment:
All

Cause:
NA

Resolution:
There is no password protection in ATS22. However, Cod parameter can be used to Lock or Unlock the parameters.
It is used to enable or disable parameters modification on the displays.
When not locked: all R/W parameters can be modified. Also accessible with key combination (ESC + UP +Down) arrow keys
When locked: all parameters are read only on local display or remote keypad display (the parameters can be still modified by serial link and SoMove software).
Was this helpful?
What can we do to improve the information ?