Technical FAQs

Ask a Question

Can 100% rated B frame breaker have EverLink lugs with Control Wire Terminal ON end?

Issue:
Can 100% rated B frame breaker have EverLink lugs with Control Wire Terminal ON end?

Product Line:
Powerpact B-Frame

Environment:
All

Cause:
Desire to use EverLink Lugs with Control Wire Terminal ON end in 100% rated B frame breaker.

Resolution:
The ever link lugs are ONLY tested/listed at 80%. They may NOT be used on a 100% rated breaker. To get a 100% rated Powerpact B frame unit mount breaker add suffixes "C" and either "LH" for AL lugs or "LC" for CU lugs.

Keywords:
Powerpact B-Frame, BD, BG, BJ, BK, EverLink Lugs, 
Control Wire Terminal, 80%, 100%
Was this helpful?
What can we do to improve the information ?