Technical FAQs

Ask a Question

Why does my Conext Combox stop logging in the middle of the night?

Issue:
Customer notices Conext ComBox stop logging every day in the middle of the night and wants to know why

Product Line:
Conext Combox 865-1058
 
Environment:
Conext Combox’s system logging and system performance graphing


Resolution:
The Conext Combox resets itself between 3:00 - 3:30AM; this is normal and cannot be disabled.

Cause:
The ComBox needs to power cycle itself on a daily basis; it will do this when solar is not available. Typically, solar is not going to be available in the middle of the night, which is why it resets at 3AM.
Was this helpful?
What can we do to improve the information ?