Technical FAQs

Ask a Question

What’s the biggest gauge (AWG) wire I can use with the supplied 60A breakers with my Conext XW+ PDP Solar Power Distribution Panel?

Issue:
What’s the biggest gauge (AWG) wire I can use with the supplied 60A breakers with my Conext XW+ PDP Solar Power Distribution Panel?

Product Line:
Conext XW+ PDP Solar Power Distribution Panel - 865-1215-01 / 865-1015-01

Environment:
Installation in which the AC wiring is too big for the 60A breakers


Resolution:
The maximum gauge (AWG) wire the 60A breaker will accept is 4 AWG

****
Torque Values for AC Disconnects and AC Breakers
Wire Size
AWG - 6-4
mm - 4.11-5.19

Torque Value
In-lb - 45
N-m - 5.1

Cause:
Wire gauge maximum not covered in PDP documentation
 
Was this helpful?
What can we do to improve the information ?