Technical FAQs

Ask a Question

Why does my Conext Battery Monitor show reverse current when I am charging?

Issue:
Customer is seeing reverse current on the battery monitor when charging with an inverter

Product Line:
Conext Battery Monitor 865-1080-01

Environment:
Conext Battery Monitor with display showing reverse current during charging and during load


Resolution:
This is a wiring issue related to the shunt sense wires. Check for proper wiring across the Violet wire (L-) and Blue wire (L+).

Cause:
Reverse polarity causing the reverse current reading
Was this helpful?
What can we do to improve the information ?