Technical FAQs

Ask a Question

How can I set up my AGS for auto EQ charging with my CSW/XW+?

Issue:
How can I set up my AGS for auto EQ charging with my CSW/XW+?

Product Line:
XW+ XW CSW AGS


Environment:
Customer cannot find a way of setting the system for auto EQ charging on the system control panel on both the inverter settings and the AGS triggers


Resolution:
The AGS will start the generator as per the trigger settings but there is not auto EQ charging

Cause:
EQ charging is not an AUTO process; this should be considered as a manual process
Was this helpful?
What can we do to improve the information ?