Technical FAQs

Ask a Question

In the ME Test Set, one of the cables is number 0677928. It needs to be replaced. Can the cable 0677928 be replaced?

Issue:
The ME Test Kit 55391 includes several cables. One of them is number 0677928. What is the replacement for that cable?

Product Line:
Circuit Breakers

Environment:
ME Test Kit number 55394

Resolution:
The cable number 0677928 is only available as part of a larger kit of accessories, kit number 34546. The 0677928 is not available by itself.
Was this helpful?
What can we do to improve the information ?