Technical FAQs

Ask a Question

M221 coil retaining its value after power cycle

Issue:
M221 coil retaining its value after power cycle

Product Line:
M221

Resolution:
In the M221, all %M bits will retain their values after a power cycle so this is normal behaviour. 
You should reset the rungs based on the %S13 (first scan bit). 
Was this helpful?
What can we do to improve the information ?