Technical FAQs

Ask a Question

Can the BSCM be used in Powerpact H J L breakers with thermal-mag or standard Micrologic trip units?

Product Line:
Powerpact H J L circuit breakers

Resolution:
PowerPact H, J and L frame circuit breakers with Standard Micrologic trip units (or thermal-mag trip units) may use a BSCM with NSX cord to report breaker status over modbus.  
The BSCM can be polled for breaker status (open, closed, tripped) but it will not be discovered by network devices such as FDM or IFE modules.
Was this helpful?
What can we do to improve the information ?