Technical FAQs

Ask a Question

Can you connect to the modbus and ULP terminals of a BCM module at the same time?

Issue:
Can you connect to the modbus and ULPO terminals of a BCM, or is it one or the other?

Product Line:
Masterpact and Powerpact P and R breakers with modbus communication

Resolution:
If you connect to the ULP terminals (E5 and E6), the modbus terminals (E3 and E4) are disabled.  
EXCEPTION:  you can connect the ULP terminals to an FDM121 and the modbus terminals to the modbus network at the same time.
Was this helpful?
What can we do to improve the information ?