Technical FAQs

Ask a Question

What would cause the ATS22 soft starters dLtA parameter to change back to dLtA after changing the setting to LINE?

Issue:
What would cause the ATS22 soft starters dLtA parameter to change back to dLtA after changing the setting to LINE?

Product Line:
ATS22

Environment:
All

Cause:
Setting the dLtA to Line and when he escapes it goes back to dLtA.

Resolution:
This is normal because the dLtA is the parameter in which the LINE setting is programmed to.  When you ESC back out you will see dLtA because the LINE setting 
is in the dLtA menu.

 
Was this helpful?
What can we do to improve the information ?