Technical FAQs

Ask a Question

How can I get pricing pricing on internally mounted SPDs for MCCs?

Issue:
How can I get pricing pricing on internally mounted SPDs for MCCs?

Product Line:
Surge Protection Device

Environment:
Product Selection

Cause:
New Installation

Resolution:
The TVS*IMA**M is a factory installed SPD for MCCs and is not available as a stand alone line item in Q2C. If you have a customer that has this unit installed inside their MCC and the front diagnostic display has a phase LED lit red then the customer needs a phase replacement module.
Was this helpful?
What can we do to improve the information ?