Technical FAQs

Ask a Question

Will the ATS22D88S6U have a built in 24vdc power supply like the ATS48 soft starter?

Issue:
Will the ATS22D88S6U have a built in 24vdc power supply like the ATS48 soft starter?

Product Line:
ATS22 and ATS48

Environment:
All

Cause:
Replaced the old ATS48 with a new ATS22...... S6U and needs the 24vdc supply

Resolution:
The ATS22 with suffix S6U will not have the +24vdc power supply like the ATS48 soft starters.  If you need the ATS22 with the built in +24vdc supply you will need to look at the ATS22 with the S6 suffix. 
 
Was this helpful?
What can we do to improve the information ?