Technical FAQs

Ask a Question

Can you use the standard pilot light lens when using an LED bulb for an XACA Pendant Station?

Issue:
Can you use the pilot standard lens when using an LED bulb for an XACA Pendant Station?

Product Line: 
Push Buttons and Operator Interface

Environment:
North American Products

Cause:
​Special lens has long lead times

Resolution:
Yes. You can mix and match lenses and bulbs either way. The only difference is in the surface of the lens.
Was this helpful?
What can we do to improve the information ?