Technical FAQs

Ask a Question

Why does the Conext CL reboot in the middle of the day?

Issue
The Conext CL reboots in the middle of the day without any indications of a fault, and all measurements look normal.

Product Line
Conext CL 18/25

Environment
Any Conext CL installation.

Cause
The Conext CL reboots every morning at 3:05 am.

Resolution
Make sure that the correct time zone is selecting during initial commissioning.  If the time zone is incorrect, the setting can be changed via the following menu:

Home Menu -> Settings -> General Settings -> Date & Time -> Select Time Zone.
Was this helpful?
What can we do to improve the information ?