Technical FAQs

Ask a Question

How do I automatically reset an undervoltage error on the LXM28A?

Issue:
How do I automatically reset an undervoltage error on the LXM28A?

Product Line:
LXM28A

Resolution:
Bit 2 of parameter P2-66 (GBIT2) with value 1 can automatically reset an Under Voltage fault. 
Was this helpful?
What can we do to improve the information ?