Technical FAQs

Ask a Question

How do you set up a ramp switch at 40hz then have a faster ramp to 60hz on the ATV630 and ATV930 process drives?

Issue:
How do you set up a ramp switch at 40hz then have a faster ramp to 60hz on the ATV630 and ATV930 process drives?

Product Line:
ATV630 and ATV930

Environment:
All 

Cause:
Wants to ramp up slow to 40hz then have a fast ramp after that to 60hz.

Resolution:
Programming to set up a ramp switch.
Complete Settings then Generic Functions
Speed Limits:
LSP =60hz
HSP= 60hz
Ramp
ACC to 30 seconds
DEC to 30 seconds
Ramp Switching
Ramp 2 frequency threshold= 40hz
Acc2= 2 seconds
Dec2= 2 seconds

 
Was this helpful?
What can we do to improve the information ?