Technical FAQs

Ask a Question

What is M241 altitude derating?

Issue:
What is M241 altitude derating?

Product Line:
TM241

Resolution:
For altitude derating, we have no curve but only a simple computed value. 
The normal ambient allowed operating temperature range is -10...+55 °C, up to 2000m 
The altitude has an influence on 2 parameters: 

- Operating temperature: temperature derating: 1 °C/400m (should be added to every 400m after 2000m)
- Insulation loss: 150 Vdc/1000m (should be added to every 1000m after 2000m)
Was this helpful?
What can we do to improve the information ?