Technical FAQs

Ask a Question

Are there any mounting restrictions on space around the ATV660 wall mounted drives?

Issue:  Can the ATV660 wall mounted drives be mounted side by side without any air gap? 
 
Product Line:   ATV660
 
Environment:  All
 
Cause:   Mounting restrictions
 
Resolution:   There are no restrictions regarding space above or below the drive. (ventilation intakes and outflow are lateral flows, not vertical)  Sides must have enough space for proper door opening
 

 
Was this helpful?
What can we do to improve the information ?