Technical FAQs

Ask a Question

Why is my Conext Combox reporting erroneous battery power?

Issue
The battery power in the System Performance section of the Combox shows extremely high values for watts after upgrading Combox firmware.

Product Line
Conext Combox, Conext XW

Environment
Legacy XW and a Combox that recently had its firmware upgraded. 

Cause:

See above, the Combox is reporting over 400kW of instantaneous power.  When the Conext Combox is on a much newer release version than the XW, the battery watts displays astronomical values.  Downgrading the firmware of the Combox actually reverts the reporting to normal values.

Resolution
The best solution is to upgrade the Conext XW to firmware v1.07.
Was this helpful?
What can we do to improve the information ?