Technical FAQs

Ask a Question

Do the CL18000NA, CL25000NA come with silicone covers for the keypads and display?

Issue: 
Customer is looking for silicon covers for our CL-18/25NA

Product Line:
Conext Inverters (CL18000NA, CL25000NA)

Environment:
CL-18/25NA

Cause:
Dislpay may not be readable after 10 years of UV exposure.

Resolution:
Silicone covers ship in the carton with the wiring box. 
 
Was this helpful?
What can we do to improve the information ?