Technical FAQs

Ask a Question

Is the HMIGXO supported by the Vijeo Designer that comes embedded with SoMachine?

Issue:
Is the HMIGXO supported by the Vijeo Designer that comes embedded with SoMachine?

Product Line:
HMIGXO

Resolution:
The HMIGXO is intended for the chinese market and is not commercialized in North America.
This is why it is not supported by the Vijeo Designer that comes embedded with SoMachine.
The standalone Vijeo Designer needs a code to unlock the HMIGXO. This code can only be obtained though chinese distributors.
Was this helpful?
What can we do to improve the information ?