Technical FAQs

Ask a Question

Where so you wire in a fire freeze stat interlock to shut down the E-Flex enclosed drive?

Issue:
Where so you wire in a fire freeze stat interlock to shut down the E-Flex enclosed drive?

Product Line:
E-Flex enclosed drive

Environment:
All 

Cause:
Wants to shut down the drive with a fire freeze stat interlock. 

Resolution:
Wiring diagrams are in the back of the E-Flex enclosed manuals.  See the attached document. 

Per the E-flex manual the shut down Fire freeze stat is terminals 1 and 2 on the HOA with bypass and without bypass 

Per the E-flex manual the shut down Fire freeze stat is terminals 1 and 2 on the no HOA and without bypass 

Per the E-flex manual the shut down Fire freeze stat is terminals 1 and 2 on the HOC with start stop and without bypass 

Per the E-flex manual the shut down Fire freeze stat is terminals A and D on the HOC without bypass.

Per the E-flex manual the shut down Fire freeze stat is terminals 3 and 3A on the HOC with bypass.
 
Was this helpful?
What can we do to improve the information ?