Technical FAQs

Ask a Question

Is there a Class 9422 operating mechanism for the Powerpact B Frame breakers?

Product Line:
9422 Cable Operating Mechanisms

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
We offer 4 lenghts, without the 9422 handle operator.

36" (914mm) Cable - 9422CSB30
60" (1524mm) Cable - 9422CSB50
70" (2134mm) Cable - 9422CSB70
120" (3048mm) Cable - 9422CSB10

Instruction bulletin NVE52880-03

Any of the following handles may be used with these operators:
9422A1
9422A2
9422A3
9422A4
 
Was this helpful?
What can we do to improve the information ?