Technical FAQs

Ask a Question

How many open TCP connections can the M221 handle?

Issue:
How many open TCP connections can the M221 handle?

Product Line:
TM221 controllers

Resolution:
The M221 slave can accept up to 8 open TCP connections. If for example the M251 acts as a master and uses 4 channels (TCP IO scanner), the M221 will have 4 open TCP connections.
Was this helpful?
What can we do to improve the information ?