Technical FAQs

Ask a Question

What is the maximum voltage for which the Conext PDP is rated?

Issue:
What is the maximum voltage for which the Conext PDP is rated?

Product Line:
Conext Power Distribution Panel

Environment:
Any XW or XW+ installation using the PDP

Resolution:
The PDP is rated for a maximum of 150DC 250AC

Cause:
Not described in data sheets for the PDP
Was this helpful?
What can we do to improve the information ?