Technical FAQs

Ask a Question

Why is my XW+ always drawing 200-300W from the grid?

Issue:
Conext XW+ inverter is always drawing 200-300W from the grid, even in grid support mode

Product Line:
Conext XW and XW+ hybrid inverter/chargers

Environment:
Any Conext XW or XW+ installation

Cause:
Feature not fully described in product documentation

Resolution:
When Sell is disabled, the XW+ pulls about 1A from the grid as a buffer to prevent accidental sell. 1A at 240V comes out to 240W, which may fluctuate a bit up and down over time.
Was this helpful?
What can we do to improve the information ?