Technical FAQs

Ask a Question

I am unable to change the AC Coupling setting on my Conext SW Solar Inverter

Issue:
Customer is commissioning a new Conext SW unit and cannot enable the AC Coupling setting

Product Line:
Conext SW
CSW4048
CSW4024
CSW2524

Environment:
Using either the Conext System Control Panel or the Conext ComBox, the CSW’s AC Coupling setting cannot be enabled. Instead, it says “value was unable to change.”
 
Resolution:
The Conext SW needs to be put in Standby mode. Once the unit is in Standby, the AC Coupling setting can be enabled.

Cause:
Some settings cannot be changed while the unit is in Operating mode.
Was this helpful?
What can we do to improve the information ?