Technical FAQs

Ask a Question

I am looking for the Pin Out for my CMR with my C Series Solar Charge Controller

Issue
Customers are looking for the Pin Out on for their CMR that installed on a C Series Solar Charge Controller

Product Line
C Series Solar Charger Controller
C60
C40
C35

Environment
Customer are using their own wiring with the CMR and need to reattach the connections at the ends of the cables.

Cause
Customers are unaware that the C-Series uses a telephony standard.

Resolution
CMR cables use a telephony standard pinout. Note that if you lay the cable flat on the table, BOTH the carpet snagger clips face UP (this is the way telephone cables were made). Note that NETWORK CABLES are opposite of this. If you laid a standard network cable 'flat' on a table, one side would have the clips facing UP while the other is facing DOWN.
Was this helpful?
What can we do to improve the information ?