Technical FAQs

Ask a Question

Can I oversize my array with the MPPT?

Issue:
Customer wants to oversized array, inputting more power then the unit can produce.

Product Line:
Conext Charge Controllers (MPPT60-150 and MPPT80-600)

Environment:
DC coupled system.

Cause:
Customer wants to harvest more solar power. 

Resolution:
 Yes, If it's within Voc and Isc (units electrical specifications)
 
Was this helpful?
What can we do to improve the information ?