Technical FAQs

Ask a Question

How to clear manual faults on the SCP (System Control Panel)?

Issue:
Customer wants to clear manual faults on the SCP (System Control Panel)

Product line:
Conext series inverters and accessories (XW, XW+, SW, AGS, MPPT, Battery Monitor)

Environment: 
Any Schneider Electric solar system

Cause:
Customer got a manual fault on one of their units

Resolution:
1. Go to device home screen using the down arrow
2. Press Enter
3. Press the down arrow until Clear Faults/Warnings is reached
4. Press Enter

Alternatively, faults can be cleared for the entire system at once.
1. From the System Status screen, press Enter
2. While highlighting System Settings, press Enter
3. Press down arrow until Clear All Faults/Warnings is reached
4. Press Enter
Was this helpful?
What can we do to improve the information ?