Technical FAQs

Ask a Question

What is the part number of the replacement fuse clip kit to convert the 9422TCF30?

Issue:
What is the part number of the replacement fuse clip kit of a 9422TCF30 so it can be used for 600V, 30A?

Product Line: 
Operating Mechanism and Disconnect Switches

Environment:
North American Products

Cause:
Would like to change the existing fuse clip

Resolution:
This comes as 30A 250V clips from the factory. 
Replacement fuse clip part number is a 9422TC33 to specifically convert to 30A 600V or 60 amp 250V fuse clips. 

More conversion information is listed below: 

Conversion Information

1.    Conversion to non-fusible:

Simply remove the fuse clips from the switchbase and mount the lugs from the fuse base assembly.  It will be necessary to remove the switchbase from the baseplate in order to remove the three fuse pullers.  The fuse pullers must be removed because they will interfere with proper placement of the lugs.

2.    Conversion to 60A 250V or 30A 600V fuse clips:

Use a Class 9422 Type TC33 Fuse Clip Conversion Kit - Line side fuse clips and a complete fuse base assembly is included.

3.    Conversion to 60A 600V fuse clips:

Use a Class 9422 Type TD63 Fuse Clip Conversion Kit - Line side fuse clips and a complete fuse base assembly is included.

4.    Conversion to 30A 250V Class R fuse clips:

Use Catalog Number RFK03.  This kit contains three Class R adapter clips, which when inserted into the existing load side fuse clips on the fuse base assembly, will reject all fuse types except Class R.  Once the adapter clips are installed, they cannot be removed.  No "Class" number is required to order this 
Was this helpful?
What can we do to improve the information ?