Technical FAQs

Ask a Question

Do I need to use the stacking port when stacking two of the Conext SW?

Issue:
Do I need to use the stacking port when stacking two of the Conext SW?

Product Line:
Conext SW

Environment:
System with two of the Conext SW inverter stacked in parallel

Resolution:
The stacking port is inactive and unnecessary for stacked Conext SW systems. Make sure the Xanbus ports are properly configured and there's a connection between the two units before starting them.

Cause:
Purpose of stacking port isn't fully explained in the CSW manual
Was this helpful?
What can we do to improve the information ?