Technical FAQs

Ask a Question

What is the replacement 5/8 socket for the handle on a racking mechanism assy for a VR breaker?

Issue:
What is the replacement 5/8 socket for the handle on a racking mechanism assy for a  VR breaker?

Product Line:
Masterclad

Environment:
Maintenance

Cause:
Replacement 

Resolution:
SQ D/ SE does not sell the 5.8 socket for the handle component separately. A new racking handle assembly, part number 4600738250, would need to be ordered
 
Was this helpful?
What can we do to improve the information ?