Technical FAQs

Ask a Question

Is Gasketing Available on The Trims on our Current Line of Hospital Isolation Panels?

Issue:
Is Gasketing Available on The Trims on our Current Line of Hospital Isolation Panels? 

Product Line:
Medical isolation panels sold and supported in the USA.

Environment:
Product Features

Cause:
Customer Inquiry

Resolution:
No option is available for gasketing on the cover/trim of our hospital isolation panelboards. 
 
Was this helpful?
What can we do to improve the information ?