Technical FAQs

Ask a Question

What does CC mean at the end of an ATV312 part number?

Issue:
What does CC mean at the end of an ATV312 part number?

Product Line:
ATV312, Altivar 312

Environment:
All

Cause:
NA

Resolution:
The CC extension is a logistic reference.
There is no impact drive reference: The product inside the package is unchanged.
Normally, the logistic reference appear only on the packaging label as indicated on the following picture. 
ATV312 Packaging label
 
Was this helpful?
What can we do to improve the information ?