Technical FAQs

Ask a Question

What's the replacement for the LXM05AD17M2 drive + SER3916 motor?

Issue:
What's the replacement for the LXM05AD17M2 drive + SER3916 motor?

Product Line:
LXM05

Resolution:
The replacement for the obsolete LXM05AD17M2 drive is a LXM32MD18M2 and a VW3M3403 encoder card. 
You can keep the motor, the power cable and the encoder cable but you need to change the connector of the encoder cable on the drive's side. 
Please note that the LXM32 does not have the same form factor as the LXM05 and adjustments to the drive's configuration have to be done. 
Was this helpful?
What can we do to improve the information ?